Zone Number (802.16 OFDMA)
: (See OFDMA Standard Presets Table.)
For multiple-zone signals, selects which zone described in the DL-MAP downlink map: A MAC message that defines burst start time for both time division multiplex and time division multiple access (TDMA) by a subscriber station (SS) on the downlink. will be analyzed. When a zone index is specified that is greater than the number of zones defined in the DL Down Link (forward link: from base station to cell phone)-MAP, the last zone described in the DLMAP will be used. Since the DL-MAP can change on every measurement, this will occur without limiting the parameter.
The performs the same function as selecting a zone on the Active Zone dropdown list for a Map File.
See Also